What are the available Security symbols?
|
Barrier |
Barrier Alarm |
|
Barrier Contact |
Blind System Alarm |
|
Card Reader |
Computer |
|
Door Contact |
Elevator Alarm |
|
Emergency Call Disabled Toilet |
Intruder Alarm |
|
Overhead Door Contact |
Pegasys Controller |
|
Repair Switch |
Swipe Reader |
|
Turnstile |
Window Contact |
What are the properties available on the Security symbols?
All Security symbols have the Shape (Circle, Square, or Triangle) Property panel properties.
All Security symbols have generic value and navigation Binding properties. The background color of the symbol is set based on the status of the value binding. The status color appears as defined in the system preferences.
All Security symbols have no snapping properties.