What are the available Pipe symbols?
|
Horizontal |
Horizontal End |
|
Diagonal |
Diagonal End |
|
Vertical |
Vertical End |
|
Front Left T |
Front Right T |
|
Front Lower T |
Front Upper T |
|
Front Upper Left Elbow |
Front Upper Right Elbow |
|
Front Lower Left Elbow |
Front Lower Right Elbow |
|
Front 4T |
Side 4T |
|
Side Left T |
Side Right T |
|
Side Lower T |
Side Upper T |
|
Side Upper Left Elbow |
Side Upper Right Elbow |
|
Side Lower Left Elbow |
Side Lower Right Elbow |
|
Top Left T |
Top Right T |
|
Top Lower T |
Top Upper T |
|
Top Upper Left Elbow |
Top Upper Right Elbow |
|
Top Lower Left Elbow |
Top Upper Left |
|
Top 4T |
Diagonal Continuation Pipe |
|
Horizontal Continuation Pipe |
Vertical Continuation Pipe |
What are the properties available for the Pipes symbols?
- System Type
- Water
- Air
- Background Color
- Pipe Type
- None
- Chilled Water Supply
- Chilled Water Return
- Condensation Water Supply
- Condensation Water Return
- Hot Water Supply
- Hot Water Return
- Condensate
- Steam
- Gas
When you apply properties to a Pipe symbol on the Graphic Canvas, any subsequent Pipe symbol placed to the Graphic Canvas retains the properties of the original Pipe symbol.
All Pipe symbols have no Binding properties.
The Pipe symbols snap to other Pipe symbols. If a Pipe symbol's system type is set to Water, than the Pipe symbols snaps to other waterside pipes. If a Pipe symbol's system type is set to Air, than the Pipe symbols snaps to other air-side pipes.