What are the available Meter symbols?
|
Electric Meter |
Gas Meter |
|
Heat Meter Horizontal |
Heat Meter Vertical |
|
Steam Meter Horizontal |
Steam Meter Vertical |
|
Water Meter Horizontal |
Water Meter Vertical |
What are the properties available on the Meter symbols?
All Meter symbols have no Property panel properties.
All Meter symbols have the generic value Binding properties.
The following Meter symbols snap to the following symbols:
| Symbol | Snaps To |
|---|---|
| Electric Meter
Gas Meter |
Pipes: Vertical and Vertical End water pipes |
| Heat Meter Horizontal
Steam Meter Horizontal Water Meter Horizontal |
Pipes: Horizontal and Horizontal End water pipes |
| Heat Meter Vertical
Steam Meter Vertical Water Meter Vertical |
Pipes: Diagonal and Diagonal End water pipes |