What are the available Chilled Beam symbols?
|
Active Chilled Beam Front |
Active Chilled Beam Back |
|
Passive Chilled Beam Front |
Passive Chilled Beam Back |
What are the Property panel properties and Binding properties available on the Active Chilled Beam Front symbol?
The Active Chilled Beam Front symbol has the following Property panel properties:
- Pipe Type:
- Two Pipe
- Four Pipe
- Coil Mode: The Coil Mode selection
is automatically set based on the Pipe Type selection. For Two Pipe, the
Coil Mode is set to Cool. For Four Pipe, the Coil Mode is set to Heat.
- Cool
- Heat
| Binding | Short Name | Animation Available |
|---|---|---|
| Water Cooling Coil Primary Value | CLG-O | Yes |
| Water Cooling Coil Secondary Value | N/A | No |
| Water Heating Coil Primary Value | HTG-O | Yes |
| Water Heating Coil Secondary Value | N/A | No |
| Navigation | N/A | No |
What are the Property panel properties and Binding properties available on the Active Chilled Beam Back symbol?
The Active Chilled Beam Back symbol has the following Property panel properties:
- Pipe Type:
- Two Pipe
- Four Pipe
- Coil Mode
- Cool
- Heat
| Binding | Short Name | Animation Available |
|---|---|---|
| Water Cooling Coil Primary Value | CLG-O | Yes |
| Water Cooling Coil Secondary Value | N/A | No |
| Water Heating Coil Primary Value | HTG-O | Yes |
| Water Heating Coil Secondary Value | N/A | No |
| Navigation | N/A | No |
What are the Property panel properties and Binding properties available on the Passive Chilled Beam Front symbol?
The Passive Chilled Beam Front symbol has no Property panel properties.
| Binding | Short Name | Animation Available |
|---|---|---|
| Water Cooling Coil Primary Value | CLG-O | Yes |
| Water Cooling Coil Secondary Value | N/A | No |
| Navigation | N/A | No |
What are the Property panel properties and Binding properties available on the Passive Chilled Beam Back symbol?
The Passive Chilled Beam Front symbol has no Property panel properties.
| Binding | Short Name | Animation Available |
|---|---|---|
| Water Cooling Coil Primary Value | CLG-O | Yes |
| Water Cooling Coil Secondary Value | N/A | No |
| Navigation | N/A | No |