Related Documentation - Metasys - LIT 12014068 - Equipment Controller - BELIMO 6-way EPIV - 1.0

Generic SA Bus for BELIMO 6-way EPIV integration Application Note

Brand
Metasys
Product name
BELIMO 6-way EPIV
Document type
Application Note
Document number
LIT 12014068
Version
1.0
Revision date
2022-06-20
Product status
Active
Language
English

Additional information concerning the Equipment Controller commissioning and setup can be found in the documentation listed in the following table

Table 1. Related documentation
For Information on Refer to
Programming and Commissioning Metasys Equipment Controllers Controller Configuration Tool (CCT) Help (LIT-12011147)
CCT and Equipment Controller Package Licensing Software Manager Help (LIT-12012389)
MS/TP Communication, SA Bus rules and specifications MS/TP Communications Bus Technical Bulletin (LIT-12011034)