Commissioning Tips - Metasys - LIT 12014068 - Equipment Controller - BELIMO 6-way EPIV - 1.0

Generic SA Bus for BELIMO 6-way EPIV integration Application Note

Brand
Metasys
Product name
BELIMO 6-way EPIV
Document type
Application Note
Document number
LIT 12014068
Version
1.0
Revision date
2022-06-20
Product status
Active
Language
English

See the following tips on commissioning a GSAB device.

Adding GSAB devices using CCT

When adding GSAB devices using CCT, the dialog window allows:

  • Application selection. When applications are available, selecting one of them is mandatory. This provides all the data points belonging to the application.
  • Point Name Prefix modification.
  • Data points selection. Points can be freely checked/unchecked as required. Note there can be dependency between points. A BACnet object can be mapped in the package more than once forming a group of points. It is possible to select no points or only one point from the group. See Point Mapping Table for group explanation.
Figure 1. Add Device dialog window in CCT

Output data points as application inputs

Read/Write Output data points can be added to Miscellaneous inputs using the EasyCAF tool. This allows output points to be duplicated on the input side so they can be used for the application.

Figure 2. Adding data point to Miscellaneous inputs in EasyCAF
Figure 3. Miscellaneous inputs in CCT