Vendor Component Requirements - Metasys - LIT 12014068 - Equipment Controller - BELIMO 6-way EPIV - 1.0

Generic SA Bus for BELIMO 6-way EPIV integration Application Note

Brand
Metasys
Product name
BELIMO 6-way EPIV
Document type
Application Note
Document number
LIT 12014068
Version
1.0
Revision date
2022-06-20
Product status
Active
Language
English

GSAB Integration for Johnson Controls Equipment Controllers and the BELIMO 6-way EPIV has been developed for the equipment shown in the following table.

Changes to this equipment or integration of BELIMO products not described in this document may require additional development and testing by Johnson Controls®.

Table 1. Ordering codes
Device Type Code
BELIMO 6-way EPIV

EP…R-R6+BAC

e.g., EP015R-R6+BAC

Documentation

6-way EPIV PICS

2021-03

belimo_BACnet_Interface-description_6way-EPIV_en-gb.pdf

Vendor Contact Information

BELIMO Automation AG

Brunnenbachstrasse 1, 8340 Hinwil, Schweiz

+41 43 843 61

info@belimo.ch

www.belimo.com