Component Requirements - Metasys - LIT 12014068 - Equipment Controller - BELIMO 6-way EPIV - 1.0

Generic SA Bus for BELIMO 6-way EPIV integration Application Note

Brand
Metasys
Product name
BELIMO 6-way EPIV
Document type
Application Note
Document number
LIT 12014068
Version
1.0
Revision date
2022-06-20
Product status
Active
Language
English

To integrate 6-way EPIV, you require the following components:

  • Properly installed and configured 6-way EPIV.
  • Programmable Equipment Controller with SA Bus interface compatible with Metasys 12.0.
  • The correct GSAB package file JC_SA_BusDevicePackages_EUR_1.1.0.xx.jcpkg, available from the license portal.
  • An interface to commission the Equipment Controller (MAP Gateway, Supervisor Passthru, direct Ethernet).
  • The following tools installed on your PC: Package Importer, CCT 15.0, EasyCAF.
  • The following licenses installed: CCT, EasyCAF, Metasys Field Controller Packages, JC SA Bus Device Packages.