Related Parts and Products - Metasys - LIT-1901050 - Supervisory Device - UL864 UUKL Listed Device - 8.1

Firefighter's Smoke Control Station (FSCS) Catalog Page

Brand
Metasys
Product name
UL864 UUKL Listed Device
Document type
Catalog Page
Document number
LIT-1901050
Version
8.1
Revision date
2017-10-01
Language
English

The FSCS panel requires the MS-FEU1610-0U Field Equipment Controller and the PAN-PWRSP-U external 96 VA Class 2 power supply. The FEU is pre-programmed by our vendor Automation Displays, Inc. (ADI) factory specifically for use with the FSCS. Any field controller reprogramming or manipulation of the controller inputs and outputs voids the UL 864 UUKL/ORD-C100-13 UUKLC 10th Edition Smoke Control Listing.