Firefighter's Smoke Control Station (FSCS) - Metasys - LIT-1901050 - Supervisory Device - UL864 UUKL Listed Device - 8.1

Firefighter's Smoke Control Station (FSCS) Catalog Page

Product name
UL864 UUKL Listed Device
Document type
Catalog Page
Document number
LIT-1901050
Version
8.1
Revision date
2017-10-01

The Firefighter's Smoke Control Station (FSCS), manufactured by Automation Displays, Inc., is a custom-built panel that provides the firefighter with monitoring and control of the building's smoke control system. The panel is a necessary and integral component for the Metasys FX system to meet Underwriters Laboratories Inc.® (UL) requirements for the UL 864 UUKL/ORD-C100-13 UUKLC 10th Edition Smoke Control Listing. Each building that has the smoke control listing requires an FSCS panel.

For important product application information regarding the use of the FSCS, refer to the Metasys® System UL 864 10th Edition UUKL/ORD-C100-13 UUKLC Smoke Control System Technical Bulletin (LIT-12012487), available from your local Johnson Controls® representative.