Description - Metasys - LIT-12011827 - Field Device - 6.0

Fan Coil Unit FCU16 Controller Product Bulletin

Document type
Product Bulletin
Document number
LIT-12011827
Version
6.0
Revision date
2013-10-15

The Fan Coil Unit FCU16 controller is a BACnet® Application Specific Controllers (B-ASC) with integral RS-485 MS/TP communications. FCU controllers integrate into the web-based Metasys® system.

The FCU16 controller features a line-voltage power supply, making this controller well suited for use in terminal units.

The FCU16 controller is designed to support fan coil unit control applications, such as:

  • Four-pipe system On/Off valve control, three-speed fan
  • Four-pipe system floating proportional valve control, three-speed fan
  • Two-pipe system On/Off valve control, three-speed fan
  • Two-pipe system floating proportional valve control, three-speed fan

Refer to the Metasys System Field Equipment Controllers and Related Products Product Bulletin (LIT-12011042) for product application details.

If the product fails to operate within its specifications, replace the product. For a replacement product, contact the nearest Johnson Controls® representative.

Figure 1. Fan Coil Unit FCU16 Controller