CAUTION
ATTENTION
CAUTION
ATTENTION
Important: Do not exceed the controller electrical ratings. Exceeding
controller electrical ratings can result in permanent damage to the controller and
void any warranty.
Important: Use copper conductors only. Make all wiring in accordance with
local, national, and regional regulations.
Important: Electrostatic discharge can damage controller components. Use
proper electrostatic discharge precautions during installation, setup, and servicing
to avoid damaging the controller.
For information on configuring and wiring a BACnet/SC or BACnet/IP network, refer to the Metasys IP Networks for BACnet/ IP Controllers Configuration Guide (LIT-12012458). For detailed information on configuring and wiring a SA Bus, refer to the MS/TP Communications Bus Technical Bulletin (LIT-12011034).