Wiring - Metasys - MS-FAC4911-0 - Field Device - FAC49 Advanced Application Field Equipment Controller - 12.0

FAC4911 Advanced Application Field Equipment Controller Installation Guide

Brand
Metasys
Product name
FAC49 Advanced Application Field Equipment Controller
Document type
Installation Guide
Part number
24-10143-1086
Document revision
E
Version
12.0
Revision date
2022-05-20
Language
English
CAUTION
  • Risk of Electric Shock:
  • Disconnect the power supply before making electrical connections to avoid electric shock
ATTENTION
  • Mise En Garde: Risque de décharge électrique
  • Débrancher l'alimentation avant de réaliser tout raccordement électrique afin d'éviter tout risque de décharge électrique.
CAUTION
  • Risk of Property Damage:
  • Do not apply power to the system before checking all wiring connections. Short circuited or improperly connected wires may result in permanent damage to the equipment.
ATTENTION
  • Mise En Garde: Risque de dégâts matériels
  • Ne pas mettre le système sous tension avant d'avoir vérifié tous les raccords de câblage. Des fils formant un court-circuit ou connectés de façon incorrecte risquent d'endommager irrémédiablement l'équipement.
Important: Do not exceed the controller electrical ratings. Exceeding controller electrical ratings can result in permanent damage to the controller and void any warranty.
Important: Use copper conductors only. Make all wiring in accordance with local, national, and regional regulations.
Important: Electrostatic discharge can damage controller components. Use proper electrostatic discharge precautions during installation, setup, and servicing to avoid damaging the controller.

For information on configuring and wiring a BACnet/SC or BACnet/IP network, refer to the Metasys IP Networks for BACnet/ IP Controllers Configuration Guide (LIT-12012458). For detailed information on configuring and wiring a SA Bus, refer to the MS/TP Communications Bus Technical Bulletin (LIT-12011034).