Input and output wiring guidelines - Metasys - MS-FAC4911-0 - Field Device - FAC49 Advanced Application Field Equipment Controller - 12.0

FAC4911 Advanced Application Field Equipment Controller Installation Guide

Product
Controls > Field Controls > FAC49 Advanced Application Field Equipment Controller
Document type
Installation Guide
Document revision
E
Version
12.0
Revision date
2022-05-20
docpartnumberlabel
Part No.
Part number
24-10143-1086

The following table provides information and guidelines about the functions, ratings, and requirements for the input and output terminals; and references guidelines for determining proper wire sizes and cable lengths.

In addition to the wiring guidelines in the following table, observe these guidelines when wiring inputs and outputs:

  • Run all low-voltage wiring and cables separate from high-voltage wiring.

  • All input and output cables, regardless of wire size or number of wires, must consist of stranded, insulated, and twisted copper wires.

  • Shielded cable is not required for input or output cables.

  • Shielded cable is required for input and output cables that are exposed to high electromagnetic or radio frequency noise.

  • Inputs or outputs with cables less than 30 m (100 ft) do not require an offset in the software setup. Cable runs over 30 m (100 ft) may require an offset in the input/output software setup.