The FAC4911 controller does not have an integral display, but you can connect it to a DIS1710 or DLK0350 Local Controller Display. If the display is configured with a local password, the equipment controller and display must be running compatible firmware versions. If the display is not configured with a local password, it is compatible with equipment controllers at any firmware version. See the following table for further details:
Display model and firmware version | Controller running 10.x firmware or greater | Controller running 9.x firmware or earlier |
---|---|---|
DLK0350 running 10.x firmware or greater | Compatible | Not compatible |
DLK0350 running 9.x firmware | Not compatible | Compatible |
DIS1710 running 6.2 firmware | Not compatible | Compatible |
For detailed information about setting up and operating a remotely connected display, refer to the DIS1710 Local Controller Display Technical Bulletin (LIT-12011270) or Local Controller Display User Guide (LIT-12013762) .