The MS -FCP-0 equipment controller firmware package files are required for CCT to configure and commission the controllers. The firmware package files also allow you to upgrade an existing XPM or IOM to the latest firmware release available for that expansion module.
Beginning at CCT Release 13, the firmware package files are orderable separately; they are not included with CCT. They are obtained from the Metasys software licensing portal, and are loaded and licensed on the computer/server that is running CCT.
For additional information about the firmware package files, refer to the CCT Installation Instructions (LIT-12011259).