Commissioning Field Controllers - Metasys - MS-FAC4911-0 - Field Device - FAC49 Advanced Application Field Equipment Controller - 12.0

FAC4911 Advanced Application Field Equipment Controller Installation Guide

Product
Controls > Field Controls > FAC49 Advanced Application Field Equipment Controller
Document revision
E
Version
12.0
Revision date
2022-05-20
docpartnumberlabel
Part No.
Part number
24-10143-1086

You commission controllers with the CCT software. The controller can be connected in one of three ways: either through Supervisor Passthru using an engine at release 9.0 or greater, MAP 4.2+/BACnet Router (Mobile Access Portal (MAP) Gateway at version 4.2 or above) or Direct Ethernet connection to the controller. Refer to the Controller Tool Help (LIT-12011147) and Controller Provisioning with Tools (LIT-12013247) for detailed information about commissioning field controllers.