Wall mount applications - Metasys - MS-FAC4911-0 - Field Device - FAC49 Advanced Application Field Equipment Controller - 12.0

FAC4911 Advanced Application Field Equipment Controller Installation Guide

Product
Controls > Field Controls > FAC49 Advanced Application Field Equipment Controller
Document revision
E
Version
12.0
Revision date
2022-05-20
docpartnumberlabel
Part No.
Part number
24-10143-1086

About this task

To mount a controller directly on a wall or other flat vertical surface, complete the following steps:

Procedure

  1. Pull the two bottom mounting clips outward and ensure they are locked in the extended position.
  2. Mark the mounting hole locations on the wall in either the horizontal or vertical mounting position. Or hold the controller up to the wall or surface in a proper mount position and mark the hole locations through the mounting clips.
  3. Drill holes in the wall or surface at the marked locations and insert appropriate wall anchors in the holes (if necessary).
  4. Hold the controller in place and insert the screws through the mounting clips and into the holes (or anchors). Carefully tighten all of the screws.
    Important: Do not overtighten the mounting screws. Overtightening the screws may damage the mounting clips.