Mounting Features and Dimensions - Metasys - MS-FAC4911-0 - Field Device - FAC49 Advanced Application Field Equipment Controller - 12.0

FAC4911 Advanced Application Field Equipment Controller Installation Guide

Product
Controls > Field Controls > FAC49 Advanced Application Field Equipment Controller
Document revision
E
Version
12.0
Revision date
2022-05-20
docpartnumberlabel
Part No.
Part number
24-10143-1086

See Figure 1 for mounting dimensions in millimeters and inches. Inches are listed in parenthesis. Figure 1 also illustrates the DIN rail channel and the mounting clips in an extended position.

Figure 1. Back of Controller