DIN Rail mount applications - Metasys - MS-FAC4911-0 - Field Device - FAC49 Advanced Application Field Equipment Controller - 12.0

FAC4911 Advanced Application Field Equipment Controller Installation Guide

Product
Controls > Field Controls > FAC49 Advanced Application Field Equipment Controller
Document revision
E
Version
12.0
Revision date
2022-05-20
docpartnumberlabel
Part No.
Part number
24-10143-1086

About this task

Mounting the controller horizontally on 35 mm DIN rail is the preferred mounting method.

To mount a field controller on 35 mm DIN rail, complete the following steps:

Procedure

  1. Securely mount a 23 cm (9.125 in.) or longer section of 35 mm DIN rail, horizontally and centered in the selected space, so that the controller mounts in the position shown in Figure 1 .
  2. Pull the two bottom mounting clips outward from the controller to the extended position.
  3. Hang the controller on the DIN rail by the hooks at the top of the (DIN rail) channel on the back of the controller, and position the controller snugly against the DIN rail.
  4. Push the bottom mounting clips inward (up) to secure the controller on the DIN rail.
    To remove the controller from the DIN rail, pull the bottom mounting clips out to the extended position and carefully lift the controller off the DIN rail.