Installation - Metasys - MS-FAC4911-0 - Field Device - FAC49 Advanced Application Field Equipment Controller - 12.0

FAC4911 Advanced Application Field Equipment Controller Installation Guide

Product
Controls > Field Controls > FAC49 Advanced Application Field Equipment Controller
Document revision
E
Version
12.0
Revision date
2022-05-20
docpartnumberlabel
Part No.
Part number
24-10143-1086

Observe the following guidelines when installing a controller:

  • To minimize vibration and shock damage, transport the controller in the original container.

  • Verify that all parts shipped with the controller.

  • Do not drop the controller or subject it to physical shock.