Input and Output terminal blocks - Metasys - MS-FAC3611 - Field Device - FAC36 Advanced Application Field Equipment Controller

FAC3611 Advanced Application Controller Installation Guide

Product
Controls > Field Controls > FAC36 Advanced Application Field Equipment Controller
Document revision
G
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-470

The fixed input terminal blocks are located on the bottom of the controller, and the output terminal blocks are located on the top of the controller. See Table 1 for more information about I/O terminal functions, requirements, and ratings.