Maximum cable length versus load current - Metasys - MS-FAC3611 - Field Device - FAC36 Advanced Application Field Equipment Controller

FAC3611 Advanced Application Controller Installation Guide

Product
Controls > Field Controls > FAC36 Advanced Application Field Equipment Controller
Document revision
G
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-470

Use Figure 1 to estimate the maximum cable length relative to the wire size and the load current (in mA) when wiring inputs and outputs.

Note: Figure 1 applies to low-voltage (<30 V) inputs and outputs only.
Figure 1. Maximum wire length for low-voltage (<30 V) Inputs and Outputs by current and wire size