About this task
Each field controller has an EOL switch, which, when set to ON, sets the controller as a terminating device on the bus. The default EOL switch position is OFF.
Figure 1. End-of-Line switch positions
To set the EOL switch on a field controller, complete the following steps: