Removing the Controller cover - Metasys - MS-FAC3611 - Field Device - FAC36 Advanced Application Field Equipment Controller

FAC3611 Advanced Application Controller Installation Guide

Product
Controls > Field Controls > FAC36 Advanced Application Field Equipment Controller
Document type
Installation Guide
Document revision
G
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-470

About this task

Important: Electrostatic discharge can damage controller components. Use proper electrostatic discharge precautions during installation, setup, and servicing to avoid damaging the controller.
Important: Disconnect all power sources to the controller before you remove the cover and change the position of any jumper or the EOL switch on the controller. Failure to disconnect power before changing a jumper or EOL switch position can result in damage to the controller and void any warranties.

The controller cover is held in place by four plastic latches that extend from the base and snap into slots on the inside of the housing cover.

To remove the controller cover, complete the following steps:

Procedure

  1. Place your fingertips under the two cover lift tabs (FAC3611 physical features) on the sides of the housing cover and gently pry the top of the cover away from the base to release the cover from the two upper latches.
  2. Pivot the top of the cover further to release it from the lower two latches.
  3. Replace the cover by placing it squarely over the base, and then gently and evenly push the cover on to the latches until they snap into the latched position.
    Figure 1. Cover removed showing EOL switch and jumper positions