Commissioning Field Controllers - Metasys - MS-FAC3611 - Field Device - FAC36 Advanced Application Field Equipment Controller

FAC3611 Advanced Application Controller Installation Guide

Product
Controls > Field Controls > FAC36 Advanced Application Field Equipment Controller
Document type
Installation Guide
Document revision
G
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-470

You commission BACnet MS/TP field controllers with the (Controller Configuration Tool ) CCT software. The controller can be connected using NxE Passthru, Bluetooth (using BTCVT), or through MAP 4.2+/BACnet Router (Mobile Access Portal (MAP) Gateway at version 4.2 or above). Refer to Controller Tool Help (LIT-12011147) for detailed information on commissioning field controllers. .

Note: The MAP Gateway serves as a replacement for the BTCVT, which is no longer available for purchase, but continues to be supported.