Wall mount applications - Metasys - MS-FAC3611 - Field Device - FAC36 Advanced Application Field Equipment Controller

FAC3611 Advanced Application Controller Installation Guide

Product
Controls > Field Controls > FAC36 Advanced Application Field Equipment Controller
Document type
Installation Guide
Document revision
G
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-470

About this task

To mount a field controller directly on a wall or other flat vertical surface, complete the following steps:

Procedure

  1. Pull the two bottom mounting clips outward and ensure they are locked in the extended position as shown in Figure 1.
  2. Mark the mounting hole locations on the wall using the dimensions in Figure 1 and one of the mount positions shown in ojb1570175964159.html#ojb1570175964159__fig_73EACA09AC7F481ABFC95E72D028500E . Or hold the controller up to the wall or surface in a proper mount position and mark the hole locations through the mounting clips.
  3. Drill holes in the wall or surface at the marked locations, and insert appropriate wall anchors in the holes (if necessary).
  4. Hold the controller in place, and insert the screws through the mounting clips and into the holes (or anchors). Carefully tighten all of the screws.
    Important: Do not overtighten the mounting screws. Overtightening the screws may damage the mounting clips.
    Figure 1. Back of Controller showing extended mounting clips, DIN rail channel, and mounting dimensions, mm (in.)