Wireless network applications - Metasys - MS-FAC2611 - Field Device - FAC26 Advanced Application Field Equipment Controller

FAC2611 Advanced Application Field Equipment Controller Installation Guide

Brand
Metasys
Product name
FAC26 Advanced Application Field Equipment Controller
Document type
Installation Guide
Part number
24-10143-187
Document revision
L
Revision date
2019-10-18
Language
English

About this task

When configured for BACnet MS/TP communication, the controller can also be installed in a wireless application using a ZFR/ZFR Pro Wireless Field Bus Router.

To configure a controller for use with the ZFR/ZFR Pro Series Wireless Field Bus system:

Procedure

  1. Wire the input/output terminals and SA bus.
    Note: In wireless network applications, do not connect any wires to the FC bus terminal block. (Connect the SA/FC terminal block on an IOM to an SA bus only.)
  2. Connect the ZFR/ZFR Pro Wireless Field Bus Router to the FC bus port (RJ-12 modular jack) on the front of the controller.
  3. Ensure that the controller's device address DIP switches are set to the correct device address. See Setting the device addresses.
  4. Set DIP switch 128 to ON, which enables wireless operation on the controller.

    For more information on the ZFR Pro Wireless Field Bus system, refer to the WNC1800/ZFR182x Pro Series Wireless Field Bus System Product Bulletin (LIT-12012320).

    For more information on the ZFR 1800 Wireless Field Bus system, refer to the ZFR1800 Series Wireless Field Bus System Product Bulletin (LIT-12011336).