Setting up a local display - Metasys - MS-FAC2611 - Field Device - FAC26 Advanced Application Field Equipment Controller

FAC2611 Advanced Application Field Equipment Controller Installation Guide

Product
Controls > Field Controls > FAC26 Advanced Application Field Equipment Controller
Document type
Installation Guide
Document revision
L
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-187

FAC2611 models do not have an integral display, but can be connected to a DIS1710 Local Controller Display. For detailed information on setting up and operating either an integral user interface or a remotely connected DIS1710 display, refer to the DIS1710 Local Controller Display Technical Bulletin (LIT-12011270) .