Wall mount applications - Metasys - MS-FAC2611 - Field Device - FAC26 Advanced Application Field Equipment Controller

FAC2611 Advanced Application Field Equipment Controller Installation Guide

Product
Controls > Field Controls > FAC26 Advanced Application Field Equipment Controller
Document revision
L
Revision date
2019-10-18
docpartnumberlabel
Part No.
Part number
24-10143-187

About this task

To mount a field controller directly on a wall or other flat vertical surface:

Procedure

  1. Pull the two bottom mounting clips outward and ensure they are locked in the extended position as shown in Figure 1.
  2. Mark the mounting hole locations on the wall using the dimensions in Figure 1 and one of the mount positions shown in Figure 1. Or hold the controller up to the wall or surface in a proper mount position and mark the hole locations through the mounting clips.
  3. Drill holes in the wall or surface at the marked locations, and insert appropriate wall anchors in the holes (if necessary).
  4. Hold the controller in place, and insert the screws through the mounting clips and into the holes (or anchors). Carefully tighten all of the screws.
    Important: Do not overtighten the mounting screws. Overtightening the screws may damage the mounting clips.
    Figure 1. Back of Controller showing extended mounting clips, DIN rail channel, and mounting dimensions, mm (in.)