Summary of changes - Metasys - LIT-12011539 - MS-EREPORT-0 - MS-EREPORT-6 - Software Application - Metasys Advanced Reporting System and Energy Essentials - 11.0

Energy Essentials Installation Guide

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System and Energy Essentials
Document type
Installation Guide
Document number
LIT-12011539
Version
11.0
Revision date
2021-01-12
Product status
Active
The following information is new or revised:
  • The latest available version of the ODS is Release 10.1. The ODS is not available for upgrade to Metasys Release 11.0.
  • Energy Essentials is no longer provided on a product disk. Instead, you can download Energy Essentials from the License Portal.