Energy Essentials overview - Metasys - LIT-12011539 - MS-EREPORT-0 - MS-EREPORT-6 - Software Application - Metasys Advanced Reporting System and Energy Essentials - 11.0

Energy Essentials Installation Guide

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System and Energy Essentials
Document number
LIT-12011539
Version
11.0
Revision date
2021-01-12
Product status
Active

Energy Essentials is an add-on to the Metasys Advanced Reporting System that focuses on the energy and utility use of your site.

Energy Essentials can run the following reports:

  • Big Picture Energy
  • Consumption
  • Electrical Energy
  • Equipment Runtime
  • Load Profile
  • Production
  • Simple Cost

For more information on how to use Energy Essentials, see Energy Essentials workflow.