Energy Essentials shares the specifications of an ADX or ODS with the Metasys Advanced Reporting System. Refer to the Application and Data Server (ADS) and Extended Application and Data Server (ADX) Product Bulletin (LIT-1201525) or Open Data Server Product Bulletin (LIT-12011943) for details.
The release number of Energy Essentials must match the release number of the ADX/ODS and the Metasys Advanced Reporting System installed on the same computer.
Note:
The latest available version of the ODS is Release 10.1. The ODS is not available for upgrade to Metasys Release 11.0.