Selection Chart - Metasys - LIT-1900600 - MS-EREPORT-0 - MS-EREPORT-6 - Software Application - Metasys Advanced Reporting System and Energy Essentials - 11.0

Energy Essentials Catalog Page

Product
Building Automation Systems > Graphics and Interfaces > Metasys Advanced Reporting System and Energy Essentials
Document type
Catalog Page
Document number
LIT-1900600
Version
11.0
Revision date
2020-10-05
Product status
Active
Table 1. Selection chart

Code number

Description

MS-EREPORT-0

Energy Essentials new project software—for new, first-time installation of Energy Essentials
Note: Requires an Extended Application and Data Server (ADX) or Open Data Server (ODS) with the Metasys Advanced Reporting System at the same release level.

MS-EREPORT-6

Energy Essentials upgrade software—for upgrading a previous Metasys release version to the current Metasys release version
Note: The Metasys release version of Metasys Energy Essentials must match the release version of ADX or ODS. If you are upgrading the ADX or ODS to and have an older release of Energy Essentials installed, you must upgrade and activate Energy Essentials. Use product code MS-EREPORT-6.
Note: Metasys Energy Essentials requires you to license the product.