|
Error or Error Message |
Solution |
|---|---|
|
The Convert to float button is disabled. |
The following scenarios could cause the Convert to float button to disable: The tool was started with a database that is already converted: If the database is already converted, you do not need to run the tool. Click Exit to exit the tool. There is not enough free disk space available: The conversion process could damage the database if there is not enough free disk space. Click Exit to exit the tool. Using Windows Explorer, manually ensure there is enough disk space available. When you determine there is enough disk space to proceed with the database conversion, start the process in Running the Data Precision Enhancement Tool again. An error has been detected: Click Show log to show error details and resolve the error. When you have resolved the error, you may continue with the database conversion. |
|
The Status field is red and displays the following message:
|
There is not enough free disk space to convert the database. The Status field lists the estimated value for the assumed required disk space. Click Exit to exit the tool. Using Windows Explorer, manually ensure there is enough disk space available. When you determine there is enough disk space to proceed with the database conversion, start the process in Running the Data Precision Enhancement Tool again. |
|
The Status field is red and displays the following message:
|
The database you are converting is too large. You must change the database from SQL Express to SQL Server and detach the database from SQL Express and attach it to the SQL Server. |
|
You receive a MPI - Warning/Hint dialog box after you attempt to convert the database. Figure 1. MPI - Warning/Hint Dialog Box
|
The tool requires permission to read the free disk space information. To resolve this problem:
|
|
The Status field is green and displays the following message:
|
The database is already converted. You do not need to run the tool. Click Exit to exit the tool. |