Running the Data Precision Enhancement Tool - Metasys - LIT-12012254 - Software Application - Metasys Database Manager - 13.0

Database Tools Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > Metasys Database Manager
Document type
Commissioning Guide
Document number
LIT-12012254
Version
13.0
Revision date
2023-10-13
Product status
Active

Procedure

  1. Browse to C:\Program Files (x86)\Johnson Controls\MetasysIII\Tools using Windows Explorer.
    Figure 1. Enhance Analog Precision Link Location

  2. Double-click the Enhance Analog Precision link to launch the Data Precision Enhancement dialog box.
    Figure 2. The Data Precision Enhancement Dialog Box

  3. Ensure that the Free disk space section of the Data Precision Enhancement dialog box is green. The green background means that there is sufficient disk space available to convert the database.
    Figure 3. Free Disk Space

  4. Click Convert to float to begin the data conversion from real to float. The fields update automatically when the conversion is complete.
    Figure 4. The Data Precision Enhancement Dialog Box after Conversion

    Notes:
    • The database conversion can take up to 4 hours to complete. See the Conversion time estimate and Progress sections of the Data Precision Enhancement dialog box (Figure 2) for the anticipated length and status of the conversion process.
    • You cannot exit the tool once the conversion process is underway.
  5. Match the field of the Data Precision Enhancement dialog box on your computer to the fields listed in Data Precision Enhancement Dialog Box after Conversion.
  6. Click Exit.