Procedure
-
Select a point in the left grid of the Convert Attribute names to IDs in the Historian Database dialog box.
Figure 1. Resolving Point Names with the Same Attribute
-
Click Resolve All (X) Point Trend(s) with the Attribute Name: (X)
with Attribute ID:.
Note: If additional points require resolution, repeat Step 1 and Step 2 until you resolve all points.
- Click Update Database and Exit to write your changes back to the database. The Successful Update dialog box appears.
-
Click OK.
Note: You need to manually restart your computer to complete the Metasys Server installation or upgrade process.