Resolving Point Names for Unknown Languages - Metasys - LIT-12012254 - Software Application - Metasys Database Manager - 13.0

Database Tools Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > Metasys Database Manager
Document type
Commissioning Guide
Document number
LIT-12012254
Version
13.0
Revision date
2023-10-13
Product status
Active

Procedure

  1. Click Skip this step and proceed or proceed with the changes already made in the Attribute Name to ID Conversion Wizard. The Convert Attribute Names to IDs in the Historian Database dialog box appears.
    Figure 1. Convert Attribute Names to IDs in the Historian Database Dialog Box

  2. If you need to resolve point names because more than one point ID exists for an attribute, go to Resolving Point Names if More Than One Point ID Exists for an Attribute. If you need to resolve point names with the same attribute, go to Resolving Point Names with the Same Attribute.