Exiting without Updating the Database - Metasys - LIT-12012254 - Software Application - Metasys Database Manager - 13.0

Database Tools Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > Metasys Database Manager
Document type
Commissioning Guide
Document number
LIT-12012254
Version
13.0
Revision date
2023-10-13
Product status
Active

About this task

Note:
  • You can exit the Attribute Name to ID Conversion tool through either the Attribute Name to ID Conversion Wizard or Convert Attribute Names to IDs in the Historian Database dialog box. The process discussed in this section applies to either window.
  • All changes made automatically by the tool or manually are lost if you exit the database without updating.

Procedure

  1. Click Cancel and Exit (lose changes). The Continue With Exit dialog box appears.
    Figure 1. Continue With Exit Dialog Box

  2. Click Yes.