Launching the Data Precision Enhancement Tool - Metasys - LIT-12012254 - Software Application - Metasys Database Manager - 13.0

Database Tools Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > Metasys Database Manager
Document type
Commissioning Guide
Document number
LIT-12012254
Version
13.0
Revision date
2023-10-13
Product status
Active

The Data Precision Enhancement tool runs after you complete the Metasys Server installation or upgrade process.

The Data Precision Enhancement tool is located in the Tools folder of the MetasysIII installation folder (C:\Program Files (x86)\Johnson Controls\MetasysIII\Tools). The folder contains the Enhance Analog Precision link. Double-click this link to launch the Data Precision Enhancement Main Page, which converts the data type in the database from real to float. See Running the Data Precision Enhancement Tool for more information on how to launch the tool.

Figure 1. Enhance Analog Precision Link Location