Data Precision Enhancement Dialog Box - Metasys - LIT-12012254 - Software Application - Metasys Database Manager - 13.0

Database Tools Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > Metasys Database Manager
Document number
LIT-12012254
Version
13.0
Revision date
2023-10-13
Product status
Active

Use the Data Precision Enhancement dialog box to convert the data type in the database from real to float. The following figure and table describe the layout of the MPI Tool for the Data Precision Enhancement dialog box.

Figure 1. Data Precision Enhancement Dialog Box

Table 1. Data Precision Enhancement Dialog Box Callouts

Callout

Description

1

SQL server version, level, and edition information.

2

Free disk space available for the database drive and the drive letter.

Notes:

  • If the .mdf and .ldf files exist on different drives, information for both drives is shown.
  • This field is not shown if the tool was started with a database that has already been converted.

3

Terminates the tool.

4

Progress for the prerequisites check and each converted table.

5

Status, warnings, and error messages pertaining to the process.

6

Starts the conversion.

The button is disabled if:

  • the tool is started with a database that has already been converted.
  • there is not enough free disk space available.
  • an error has been detected.

7

MPI.log file with conversion details.

8

Required conversion time estimate.

9

Number of analog rows.

10

State of the data type throughout the process. For example, this field may contain SQL real or SQL float.

11

Database .ldf file size in MB.

12

Database .mdf file size in MB.

13

Database name from the connection string.

14

SQL server name from the database connection string.