Data Precision Enhancement Dialog Box after Conversion - Metasys - LIT-12012254 - Software Application - Metasys Database Manager - 13.0

Database Tools Commissioning Guide

Product name
Metasys Database Manager
Document type
Commissioning Guide
Document number
LIT-12012254
Version
13.0
Revision date
2023-10-13
Product status
Active

The layout of the Data Precision Enhancement dialog box changes after the database conversion is complete. The following figure and table describe the layout of the Data Precision Enhancement dialog box after the conversion occurs.

Figure 1. Data Precision Enhancement Dialog Box after Conversion

Table 1. Data Precision Enhancement Dialog Box after Conversion Callouts

Callout

Description

1

SQL server version, level, and edition information

2

Displays the actual value

3

Terminates the tool

4

Displays progress in green

5

Done

6

Disabled

7

MPI.log file with conversion details

8

SQL float

9

Displays the actual value

10

Displays the actual value

11

Database name from the connection string

12

SQL server name from the database connection string.