Use the Data Precision Enhancement dialog box to convert the data type in the database from real to float. The following figure and table describe the layout of the MPI Tool for the Data Precision Enhancement dialog box.
Callout |
Description |
---|---|
1 |
SQL server version, level, and edition information. |
2 |
Free disk space available for the database drive and the drive letter. Notes:
|
3 |
Terminates the tool. |
4 |
Progress for the prerequisites check and each converted table. |
5 |
Status, warnings, and error messages pertaining to the process. |
6 |
Starts the conversion. The button is disabled if:
|
7 |
MPI.log file with conversion details. |
8 |
Required conversion time estimate. |
9 |
Number of analog rows. |
10 |
State of the data type throughout the process. For example, this field may contain SQL real or SQL float. |
11 |
Database .ldf file size in MB. |
12 |
Database .mdf file size in MB. |
13 |
Database name from the connection string. |
14 |
SQL server name from the database connection string. |