Convert Attribute Names to IDs in the Historian Database Dialog Box - Metasys - LIT-12012254 - Software Application - Metasys Database Manager - 13.0

Database Tools Commissioning Guide

Product
Building Automation Systems > Databases and Data Servers > Metasys Database Manager
Document number
LIT-12012254
Version
13.0
Revision date
2023-10-13
Product status
Active

The Convert Attribute Names to IDs in the Historian Database dialog box allows you to interact directly with the point names when you are unsure which language the trend samples are stored in, or if the number of point names requiring resolution indicated in the Attribute Name to ID Conversion Wizard is greater than 0 after attempting to resolve all points.

The following figure shows an example of the Attribute Name to ID Conversion Dialog after you have left the Attribute Name to ID Conversion Wizard. The buttons and features of the dialog are described in detail in the table following the figure.

Figure 1. Convert Attribute Names to IDs in the Historian Database Dialog Box

Table 1. Convert Attribute Names to IDs in the Historian Database Dialog Box Callout

Callout

Description

1

Table from which to choose attribute IDs (if necessary).

2

Resolves an individual point with the same attribute name.

3

Resolves all points with the same attribute name.

4

Updates the JCIHistorian database.

5

Closes the dialog box without saving.

6

Reverses all changes and rereads the current contents of the JCIHistorian database.

7

Indicates how much of the process is completed.

8

Table showing the point names and attribute of the JCIHistorian database.

9

Opens the log file.