The Attribute Name to ID Conversion Wizard resolves and merges all point names in the trend database. The wizard is activated when you select the Convert Attribute Names to IDs for Trend link in the MetasysIII installation folder previously discussed in Launching Attribute Name to ID Conversion Tool.
The wizard automatically resolves all point names with attribute names in US English. The tool also manually resolves and merges point names with non-English attribute names.
Figure 1 shows an example of the Attribute Name to ID Conversion Wizard when it has been launched. The button options are described in detail in Table 1.
|
Callout |
Description |
|---|---|
|
1 |
Shows available conversion languages. |
|
2 |
Resolves the points for all attributes with the language selected in the drop-down box immediately above it. This can be used when you know the language the trend samples are stored in. You need to select a language from the drop-down box before you click the button. |
|
3 |
Exits the wizard to continue the conversion process with the Convert Attribute Names to IDs in the Historian Database dialog box. Use this when you are unsure which language the trend samples are stored in, or the number of point names requiring resolution indicated is greater than 0. |
|
4 |
Writes any changes back to the database. Note: The wizard only writes changes back to the database if you click Update Database
and Exit. The wizard does not automatically write
these changes back during the process.
|
|
5 |
Cancels any changes and closes the wizard. |
|
6 |
Opens the log file. |