Power Supply Connection - Metasys - DARKNODE-PNL-0 - Control Panel - DarkNode Panel - 8.0

DarkNode Panel Installation Instructions

Product
Enclosures, Mounting and Panels > Control Panels > DarkNode Panel
Document revision
A
Version
8.0
Revision date
2020-02-25
Product status
Discontinued
Part number
24-10948-2

Follow these important guidelines:

  • Route AC power wiring through the knockout located on top of the panel.
  • Connect the AC power wiring to terminal block TB-1.
  • Do not connect the DC power cable to the DarkNode module until all wiring is complete.