WARNING
Important: Make all wiring connections in accordance with local, national, and regional regulations. Do not exceed the DarkNode Panel's electrical rating.
Important: Use only unshielded Ethernet cable in order to prevent electrical ground loops and reduce Electro-Magnetic Interference (EMI).
The DarkNode Panel includes a terminal block (TB1) for routing 120 VAC to the 24 VDC power supply. The following figure shows the wiring inside the DarkNode Panel.
Figure 1. DarkNode Panel Internal
Wiring