Location Considerations - Metasys - DARKNODE-PNL-0 - Control Panel - DarkNode Panel - 8.0

DarkNode Panel Installation Instructions

Product
Enclosures, Mounting and Panels > Control Panels > DarkNode Panel
Document revision
A
Version
8.0
Revision date
2020-02-25
Product status
Discontinued
Part number
24-10948-2

Follow these guidelines when mounting the DarkNode Panel:

  • Select a network room location that is secure and adjacent to the server or workstation.
  • Ensure that the mounting surface can support the enclosure.
  • Ensure the door can swing fully open.
  • Use the pre-punched knockouts as entrance points for the cables and wires.
  • Select a location where airflow is uninhibited over the exposed surfaces.
  • Remove the back plate from the panel by removing the four fasteners that hold the plate in place.
  • Mount the panel on a wall or other mounting surface located in a restricted-access area.
  • Replace the back plate after the panel mounting is complete.