Follow these guidelines when installing the DarkNode Panel:
- Transport the panel in the original container to minimize vibration and shock damage.
- Verify that all the parts shipped with the panel.
- Do not drop the panel or subject it to physical shock.
- Do not remove the DarkNode module from the panel for the purpose of installing the module in a non-secure location. The DarkNode module must remain in the panel to pass agency listing and to protect the module connections from tampering.
If you need details about how to commission the DarkNode Panel after installation, contact your local Johnson Controls® representative.