Application - Metasys - DARKNODE-PNL-0 - Control Panel - DarkNode Panel - 8.0

DarkNode Panel Installation Instructions

Product
Enclosures, Mounting and Panels > Control Panels > DarkNode Panel
Document revision
A
Version
8.0
Revision date
2020-02-25
Product status
Discontinued
Part number
24-10948-2

The DarkNode® Panel is a pre-wired, preassembled standard control panel and enclosure that contains a DarkNode Module with embedded encryption technology for use on a building automation system network. The control panel is shipped complete and mounted in a steel enclosure. The panel is equipped with a 120 VAC/24 VDC power supply.

The DarkNode Panel is designed specifically for use on the Metasys Server or BACnet® Operator Workstation (B-OWS) side of an encrypted network. The enclosure has a lift-off door and a lockable door with key.

Figure 1. DarkNode Panel